Query Only
:CALCulate:TRACe{Tr}:DTIMe:DATA?
This command gets delta time result value. You can get the result even if :CALCulate:TRACe{Tr}:DTIMe:STATe is off.
|
Description |
Value of delta time result. |
|
Data Type |
Double precision floating point type (Double) |
|
Range |
- |
|
Preset Value |
- |
|
Unit |
- |
|
Resolution |
- |
{numeric}<newline><^END>
10 OUTPUT 717;":CALC:TRAC1:DTIM:TARG 5"
20 OUTPUT 717;":CALC:TRAC1:DTIM:POS 50"
30 OUTPUT 717;":CALC:TRAC1:DTIM:DATA?"
40 ENTER 717;A
:CALCulate:TRACe{Tr}:DTIMe:POSition
:CALCulate:TRACe{Tr}:DTIMe:STATe
:CALCulate:TRACe{Tr}:DTIMe:TARGet
No equivalent GUI is available.